CodeWarrior for Microcontrollers v10.x Project XML

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior for Microcontrollers v10.x Project XML

ソリューションへジャンプ
1,986件の閲覧回数
mjosborne
Contributor II

Hi there,

 

I was wondering if there is any support for the import/export of .project XML files?

I'm using the CodeWarrior Classic Project Importer wizard to import an existing Coldfire project .mcp from 5.9.0, which is fine.

 

However, once I have converted the project I would like to generate an XML description that can be placed under version control and used by other developers so they don't have to perform the project conversion themselves.

 

Is this possible (or is there a better way that I don't know about being a first-time user of the Eclipse-based IDE)?

 

Thanks for the help,

 

Matt.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,618件の閲覧回数
CrasyCat
Specialist III

Hello

 

The files .project and .cproject that are created after importing a project into CodeWarrior V10.x are in fact XML files.

 

You should be able to check them in into VCS.

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,619件の閲覧回数
CrasyCat
Specialist III

Hello

 

The files .project and .cproject that are created after importing a project into CodeWarrior V10.x are in fact XML files.

 

You should be able to check them in into VCS.

 

CrasyCat

0 件の賞賛
返信
1,618件の閲覧回数
mjosborne
Contributor II

So the one time conversion deals with the binary mcp file and then it's all XML - that's exactly what I was hoping for.

 

Thanks for the help.

 

-Matt.

0 件の賞賛
返信