CodeWarrior for 68K debug interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior for 68K debug interface

3,891 Views
stefanorocca
Contributor II
Hello,
I'm using CodeWarrior for 68K/Codlfire Embedded System IDE version 4.2.7.593 (seems to be the last, purchased one week ago).
My target is a MC68332 processor.
 
I purchased a P&E UB CPU16/32 MULTILINK (usb bdm interface) in order to debug, but the IDE doesn't support it.
Is there any update/patch for doing that?
If not, may you suggest me some interfaces that really work with you IDE?
 
Thank you in advance.
 
Stefano
Labels (1)
0 Kudos
Reply
3 Replies

1,961 Views
CrasyCat
Specialist III
Hello
 
CodeWarrior for 68K supports parallel cable from P&E only.
So what you need is a CABLE_16/32 or a CABLE_16/32LV from P&E.
 
CrasyCat
0 Kudos
Reply

1,961 Views
stefanorocca
Contributor II
Thanks CrasyCat,
 
I got the parallel interface.
It seems to work only on the PCs equipped with a parallel port on the main board.
With the others (all the actual PCs, w/o parallel port on the main-board, but added as a PCI add-on),  it doesn't work.
Is it right?
 
Stefano
 
0 Kudos
Reply

1,961 Views
CrasyCat
Specialist III
Hello
 
I am not sure this can work.
 
I would suggest you to contact P&E and ask them whether they have a solution for that.
They have a forum as well at following URL:
CrasyCat
0 Kudos
Reply