CW_68K_V3.2.exe (codewarrior for the 68K)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW_68K_V3.2.exe (codewarrior for the 68K)

2,699 次查看
stefanorocca
Contributor II
Hello to All,
 
I purchased  CWA-PRO-FL instead of a CWA-PRO-NL: my PC is not a server.
While I'm waiting for a solution from the support, I need to start to work on it immediately.
 
For solving this situation (and while the support replis me), I downloaded the trial version (valid for 30 days) of the codewarrior for the M68K.
 
Despite the information, no license is contained: the license.dat file is empty and the program doesn't run.
Can someone help me?
 
Stefano 
标签 (1)
0 项奖励
回复
2 回复数

1,223 次查看
stefanorocca
Contributor II
Problem solved.
 
The Customer Support changes my license to a node locked (NL) version.
 
Stefano
0 项奖励
回复

1,223 次查看
J2MEJediMaster
Specialist I
Glad to hear you got the licensing issue solved. And you did the right thing, which is worth pointing out here.

We've got an automated system that doles out CodeWarrior licenses. As developers, you know that occasionally such a complex system can misfire. When that happens, in order get you a working license as fast as possible--as well as bring the error condition to our attention so that the automated system can be improved--it's best to file a Service Request (SR) on any licensing problem.

---Tom
0 项奖励
回复