Changing subject back to the linux issue - I've run into the same issue with Fedora Core 8, same error message in the original thread, running the 9.2 Linux Platform Edition for Mobile GT.
     Any resolution for running on FC 8? This is actually the 2nd workstation I've set up for development (different/worse/simlar failure on FC 10), hate to install another version just to have the same result...
     CW says it requires red hat enterprise 3 or 4, and doing a quick google search turns up the wikipedia entry for read hat enterprise - that says rhe4 is based on FC 3. So... does it for sure work on FC 3 then, and no other/newer FC version?
      Thanks in advance,