CodeWarrior(TM) Development Studio V8.8 Connection Issue on New PC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior(TM) Development Studio V8.8 Connection Issue on New PC

Jump to solution
1,905 Views
nitheeshkumar
Contributor I

Dear [Support/Team],

I am using the MPC8358E chip for my project. The software code for this project was originally developed in early 2016 on a Windows XP PC (let’s call it the reference PC). I was not the original developer.

Now, I need to make some modifications to the code for my new design. I have moved to a Windows 11 (64-bit, 8 GB RAM) PC (let’s call it the new PC).

I downloaded and installed CodeWarrior™ Development Studio for Power Architecture™ Processors V8.8 from the NXP website. Using this tool, I can run hardware diagnostics to check the hardware connection. However, when I connect using my new PC, I am getting an error indicating that the hardware is not connected.

Below i am share the screenshot  for your reference Screenshot (40).png

When I connect the same hardware setup to the reference PC, it connects successfully. This confirms that both the hardware and the JTAG interface are working correctly.

I have copied and verified the IDE preferences and target settings (for both Debug and ROM versions) from the reference PC to the new PC. Everything seems correct, but I still face this connection problem.

Please help me resolve this issue, as I need to complete the project by the end of this month.

Best regards,
NKJ

0 Kudos
Reply
1 Solution
1,872 Views
Oswalag
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
2 Replies
1,873 Views
Oswalag
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
1,837 Views
nitheeshkumar
Contributor I
hello,
NXP Tec support,
The link is not opening. If you meant that link have 8.8.6 Patch file, I’ve already installed everything as suggested, but I’m still experiencing the same issue.
0 Kudos
Reply