CodeWarrior 8 on Mac

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,270件の閲覧回数
cultana
Contributor I

I have been using CW development tools v8.3 in Windows for a while. I wanted to move some work to my Mac platform options. These are the desktop versions of CW.

Unfortunately I did not get the updates for the Mac version

 

1. I am assuming the updates for the Mac OS as per this ref:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MAC

are for the desktop version.

 

2. I have the following hardware/Mac OS configs and I am not sure which the Mac version works under.

a.) iMac Intel Core 2 Duo: OS 10.5.8

b.) iMac Power PC G4: OS 10.4.11/OS9.2,– has the option of either OSX or Classic OS.

c.) Power Mac G3 OS 9.2.2 – Already has CW Pro 5 and CW Pro 7 depending on startup

 

3. Before I go off and upgrade/patch the Mac 8.0 to 8.3 does it require the license file. If so how do I get this license code back as I registered my original CW product way back, about CW Pro Release 1, and I have only been getting the ‘Renewal’ versions. The original license file was lost with a computer crash years ago.

 

I want to move back to the Mac preferably the G4 or G3 as I am doing some ugly pointer to pointer to pointer and so on work. The Mac is a bit easier, particularly the G3/G4, to do some debug work vs Windows.

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
2,537件の閲覧回数
J2MEJediMaster
Specialist I

Freescale no longer supports the desktop version of the CodeWarrior tools for Mac and Windows. The CodeWarrior tools are for embedded development only.

 

Having said that, I will try to answer your questions, but don't expect them to be accurate (I am trying to recall six-year old details here), nor can I offer any follow-up support.

 

1) I do not know.

 

2) I think version 9 of the CodeWarrior tools might have run under Mac OS X, but I am not sure. Your best bet is to run CW under Mac OS 9. Any Mac that can run Mac OS 9 will do. That rules out the Intel Mac.

 

3) If CodeWarrior is still working on the Mac, you have a valid license file. Updating the tools from v8 to v8.3 should not require a new license. Make a copy of the license.dat file in the CodeWarrior folder before updating anything.

 

---Tom

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,538件の閲覧回数
J2MEJediMaster
Specialist I

Freescale no longer supports the desktop version of the CodeWarrior tools for Mac and Windows. The CodeWarrior tools are for embedded development only.

 

Having said that, I will try to answer your questions, but don't expect them to be accurate (I am trying to recall six-year old details here), nor can I offer any follow-up support.

 

1) I do not know.

 

2) I think version 9 of the CodeWarrior tools might have run under Mac OS X, but I am not sure. Your best bet is to run CW under Mac OS 9. Any Mac that can run Mac OS 9 will do. That rules out the Intel Mac.

 

3) If CodeWarrior is still working on the Mac, you have a valid license file. Updating the tools from v8 to v8.3 should not require a new license. Make a copy of the license.dat file in the CodeWarrior folder before updating anything.

 

---Tom

 

 

0 件の賞賛
返信
2,537件の閲覧回数
cultana
Contributor I

Tom,

Thanks for the info.

 

"I am trying to recall six-year old details here" ... Heck that long ago, I lost track of CW after the Uni I was working at switched to teaching Java instead of C++ and CW as getting left behind in Java.

 

As for embedded, sorry not my league, its all dektop mil tac sim tools  this end.

 

As it is, I am only using CW as a base tool to iron out issues with code the actuall updates for v8 are not critical. I do have a working v5 and 7 Pro on the OS 9.2 Mac. The main work is in Microsoft VS with or without a GUI tool like Qt or Zinc.

 

Having v8 running under OSX would just save switching OS each time I needed to use CW, but not mission critical.

 

With respect to the CW 8.1 - 3 updates they appear to be of the size for the desktop version based on some comments I have seen elsewhere.  

Anyway I can but try and see.

 

Again thanks.

Nick

 

 

 

 

 

.

 

0 件の賞賛
返信