CodeWarrior 6.4 known issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior 6.4 known issues

1,172件の閲覧回数
mstephenson
Contributor I

We are using legacy CodeWarrior 6.4 for ColdFire under Windows. Compiler release notes indicate "6.4 build 0002". I have release notes from 2007 but I would like to know if there is a more recent set of release notes for this software. I cannot find anything on the public Freescale website regarding this tool. The Documentation page does not list software tools as an option, only devices.

 

I realize that this tool is no longer supported so if release notes and known issues lists and errata are not being maintained (i.e. i have the latest), that is an acceptable answer. If nothing else, is there an area of the Freescale website dedicated to known issues and release notes for all software products?

ラベル(1)
0 件の賞賛
返信
1 返信

1,021件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

I attached the release note for CW6.4 and CW7.1.  You can see the changes and bug fixes in CW7.0 & 7.1 in CW7.1 release note.

Best Regards

Fiona

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信