CodeWarrior 6.1 Go to macro declaration error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior 6.1 Go to macro declaration error

3,167件の閲覧回数
RodBristol
Contributor I
When a macro is conditionally compiled and the file holding the declaration is not open, the right-click-and-Go-to-macro-declaration feature works correctly. If the file holding the macro is already open, the IDE chooses the last declaration in the file instead of the correct one. This is with the "Generate Browser Data From Compiler" option selected.
 
In my project, the compile switches are defined in a file set on a path unique to each target.
 
Here's an example:
/* active high relay control on port E */
#if(LocalRelayDrive == 1)
#define SetLocalRelayOn         PTED |= 1
#define SetLocalRelayOff        PTED &= ~0X01
#define GetLocalRelayStatus     (PTED & 1)
/* active low relay control on port E */
#elif(LocalRelayDrive == 0)
#define SetLocalRelayOff        PTED |= 1
#define SetLocalRelayOn         PTED &= ~0X01
#define GetLocalRelayStatus     (!(PTED & 1))
/* multiple relay control  on port B */
#elif(LocalRelayDrive == 3)
#define ShutdownRelayOff        PTBD |= (1<<2) // brown, shutdown
#define ShutdownRelayOn         PTBD &= ~(1<<2)
#define SetLocalRelayOff        PTBD &= ~(1<<1) // gray, short = setback
#define SetLocalRelayOn         PTBD |= (1<<1) // open = occupied
#endif
 
 
Thanks.
Rod Bristol
 
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,387件の閲覧回数
CrasyCat
Specialist III
Hello
 
I would recommend you to submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.
 
CrasyCat
0 件の賞賛
返信

1,387件の閲覧回数
RodBristol
Contributor I
Packed and sent. Thanks.
Rod Bristol
0 件の賞賛
返信