Code Warrior HC08 Compiler Error: C2801: 'while' missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warrior HC08 Compiler Error: C2801: 'while' missing

1,583 Views
Aniljaganath
Contributor I

Hi,

I am using code warrior for first time.

 

I am facing this error during my code compilation:

 

This points to my this function first line.

I am not able to understand what is this about?

 

 

Code

=========================================

void FlashEraseRestart(uint16 startAddr, uint16 size)
{
   FlashOpStatus status = FLASH_OP_OK;
   uint32 addr = startAddr;
   if(addr >= FLASH_START_ADDRESS)
   {
      //Disable Interrupts. Access to flash during flash operations is not allowed
       asm
       {
           SEI;
       }
      for(addr = startAddr; addr < (startAddr + size - 1UL); addr += FLASH_SECTOR_SIZE)
      {
          //Erase 1 sector at a time
          status = u8Flash_Erase((uint16)addr);
          if (FLASH_OP_OK != status)
          {
             break;
          }
      }
      //Enable interrupts
      asm
      {
          CLI;
      }
   }
   else
   {
      status = FLASH_OP_ERROR;
   }
   return status;
}

Labels (1)
0 Kudos
Reply
1 Reply

1,252 Views
CompilerGuru
NXP Employee
NXP Employee

Not sure which line you refer to with "first line", the function prototype?

Anyhow, for such errors I would recommend to generate a preprocessor listing and then compile that.

In the code below, I guess there are at least some macros hidden, maybe one more than you think due to a name collision.

Also if the error is on the function prototype, the error might be in the stuff before the shown function.

Daniel

0 Kudos
Reply