Cannot read CodeWarrior Dongle

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cannot read CodeWarrior Dongle

1,881 次查看
keithtang
Contributor IV

I received the CodeWarrior Dongle from Freescale and followed the procedure here:

http://cache.freescale.com/files/soft_dev_tools/doc/support_info/DongleQS.pdf?WT_TYPE=Supporting%20I...

 

to install the driver and imtools to read the FLEX ID without success. I have tried on both Windowx XP and 7, both with no luck. The FlexID box simply just blank.

 

The dongle appears to be a flash drive with size of 10GB, with 5.3GB used .There is only one main folder, labelled CodeWarrior_Supporting_Folders, with sub folders. No flashing LED as described.

 

I am describing this in detail hoping someone can tell me if this a dongle or just a orniary flash drive. If it is a dongle, what has possibly gone wrong and how do I troubleshoot.

 

Thanks.

标签 (1)
0 项奖励
回复
7 回复数

1,648 次查看
J2MEJediMaster
Specialist I

You need to file an on-line service request for a licensing problem. Click here to do that.

 

---Tom

0 项奖励
回复

1,648 次查看
keithtang
Contributor IV

Thanks.

 

In fact I have already done that just after posting this message. I just thought of getting quick solution, as this seems to be a common problem among the developers.

0 项奖励
回复

1,648 次查看
keithtang
Contributor IV

Latest update from the support team. It seems that the USB thumb drive they shipped out is NOT a dongle, rather just a thumb drive. I am not sure why they do not use CD but thumb drive, which confused me.

 

Apparently I need to purchase the dongle separately, which costs USD99.

0 项奖励
回复

1,648 次查看
J2MEJediMaster
Specialist I

Thanks for the update. I am sorry it took this long to find the real problem.  Did they give you a temporary license so that you could work while the problem was being investigated?

 

---Tom

0 项奖励
回复

1,648 次查看
keithtang
Contributor IV

Its OK, life is full of unexpectation. :smileywink:

 

Thanks for reminding me. I have just sent an email to request for extension to my current 30 days evaluation copy, which is coming to the end soon.

 

By the way, one question. Do I have to uninstall my current evaluation copy before installing the licensed copy? I have to say the installation / uninstallation process was not something I would like to repeat when given a choice.

0 项奖励
回复

1,648 次查看
CrasyCat
Specialist III

Hello

 

No.

For CodeWarrior V10.x just copy your new license.dat file to the {Install}\<TARGET> directory (where {Install} stands for your installation directory).

 

If you are using CodeWarrior for MCU, the license.dat must be copied in {Install}\MCU.

If you are using CodeWarrior for Power Architecture, the license.dat must be copied in {Install}\PA.

If you are using CodeWarrior for StarCore, the license.dat must be copied in {Install}\SC.

 

For earlier version of CodeWarrior copy the license file to your installation directory.

 

CrasyCat

0 项奖励
回复

1,648 次查看
keithtang
Contributor IV

Thank you, CrasyCat, for the info.

 

Received the dongle from Digikey, brilliant. Installed, tested, activated OK. I don't need to extend the evaluation copy, which expired yesterday.

0 项奖励
回复