Can we change the default parallel port address  in codewarrior 4.0.2?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can we change the default parallel port address  in codewarrior 4.0.2?

2,365 次查看
sheyue
Contributor I

There are not parallel port in My notebook. So I use a "PCMICA TO PARALLEL PORT CARD". But its address is not 0x378,0x278 and 0x3bc, and it can not change the address of lpt1,lpt2 and lpt3. 

So I should change the parallel port address in codewarrior. I know we can change it in ccs. But I am using codewarrior 4.0,there are not ccs. So I want to know Can we change the default parallel port address in codewarrior 4.0.2?

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

842 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

 

I got some info from our development team.

We dont have solution with DSP v4.0.

 

I recommend you to use the last version

  CodeWarrior for DSC56800E v8.2.3

 

You can download this version on our web site via the link:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC

For details please have a look in:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC&tab=In-Depth_Tab

In the download tab you can download the Special Edition or the Evaluation.

The Special edition contains the special edition license limited to 32 kb of Code.

We recommend you to download the Evaluation edition.

A Professional Evaluation license is provided for first 30 days.

After 30 days the product will function at the Special Edition level.

If you need another version of the license please contact your local distributor.

You can purchase it directly from the web site too.

We changed the pricing and packaging structure for Codewarrior Tool.

Now there are 4 suites:

special (free version)

basic

standard

professional

Please refer to the link for details:

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127262E703BC5

 

Regards

Pascal

0 项奖励
回复

842 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

 

CodeWarrior for DSP V4.0 was released in 2000.

This is an old version.

I don't know if it's possible to change the port.

I will try to contact some guys in development team.

Keep you informed.

 

Regards

Pascal

0 项奖励
回复