CWHC08 V6.1 Project window pull down list

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CWHC08 V6.1 Project window pull down list

3,341件の閲覧回数
wre
Contributor III
Hi!  In prior versions of CW, the pull down list in the project window was a list of targets.  In a project created with 6.1 the list is a list of Connections.  A project created with v3.1 but opened in v6.1 has the list of targets in the pull down (desired result).
 
Is there a way to change the pull down list to be the list of targets rather than connections?
 
Thanks,
 
Bill
 
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,510件の閲覧回数
CrasyCat
Specialist III
Hello
 
The Technical note TN241 includes a section called "Using Build Targets" which explains that.
You should be able to find this Technical Note in {Install}\Help\PDF directory.
 
I hope this helps.
 
CrasyCat
0 件の賞賛
返信

1,510件の閲覧回数
wre
Contributor III
Thanks, that did help.  I use different "targets" for building release or debug flavors of the application and it is far more convenient to use the pull down.
 
Bill
 
0 件の賞賛
返信

1,510件の閲覧回数
udragon
Contributor I
I tried the same thing in CodeWarrior 6.2 and it works fine, however when I close & reopen a project the target list disappears again.
 
Note I already checked that :
 
- the .prefs file is NOT readonly
- I have full rights to "program files\Freescale"
- I clicked save in the "custimize ide commands" window.
 
Maybe a bug in CW 6.2 (ide 5.9?? )
0 件の賞賛
返信

1,510件の閲覧回数
CrasyCat
Specialist III
Hello
 
This is working fine for me.
I suppose there is an issue with your configuration.
 
Do you have read/write access to your whole CodeWarrior installation directory?
 
I would recommend you to submit a service request to get a support engineer to look at that..

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.
 
CrasyCat
0 件の賞賛
返信