CW8 ProcExp - 56F8357 - problem PWM control

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW8 ProcExp - 56F8357 - problem PWM control

5,323件の閲覧回数
howdeterminepwm
Contributor I
HI,
I cant ON PWMA5 in Demo Board. I can enable all PWM's A0-A4 except A5. I have using Processor Expert, and Code Warrior not returns error. Other problem, enabling one PWM, all PMW's is ON, example:
ACTION: Enable PMWA0
RESULT: Enable PWMA0, PWMA1, PWMA2, PWMA3, PWMA4 (except five)

ACTION: Press IRQB for disable PWMA0
RESULT: Disabled PWMA0, and no change for others

How enable PWM5 and no enable all?


Message Edited by Alban on 2007-09-20 09:29 AM
ラベル(1)
タグ(1)
0 件の賞賛
返信
6 返答(返信)

2,545件の閲覧回数
Alban
Senior Contributor II
Hello,

Have you read this post, by any chance ?

[IMPORTANT] When Asking about CODEWARRIOR !!!

Regards,
Alban.
0 件の賞賛
返信

2,545件の閲覧回数
howdeterminepwm
Contributor I
Sorry, where edit topic??
Thank you!
0 件の賞賛
返信

2,545件の閲覧回数
J2MEJediMaster
Specialist I
Every time you post, you need to supply the CPU type and CodeWarrior version in the subject header. You're talking details about a PWM, but since many Freeacale CPUs have these, no one has an idea what part you're talking about. I've seen you post before with this information. I'm assuming that you're still using DSP56800/code warrior 8 with a 8357? Just keep in mind not everyone is going to read every post in the forum, and so you have to provide the information each time.

---Tom
0 件の賞賛
返信

2,545件の閲覧回数
howdeterminepwm
Contributor I
Sorry, my cpu is 56f8357 and code warrior is version 8, using Processor Expert (PE). You're correct Tom.


Message Edited by how determine pwm frequency on 2007-09-19 03:49 PM

Message Edited by Alban on 2007-09-20 09:29 AM
0 件の賞賛
返信

2,545件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
Can I suggest you to log this question in our CRM system ?
The problem must be handle by our support team and may be our Third Party Unis.
 
Please use Freescale on line support web page.
  - Go to following URL: http://www.freescale.com/TechSupport
  - Click on Submit a Service Request. You will come to a login page.
  - You can submit your request through the web from there.
There is a patch for the DSC8.0 (must be installed in first) DSC8.1.1
You can download it on our web site via the link:
 http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600617882140B
Regards
Pascal Irrle
0 件の賞賛
返信

2,545件の閲覧回数
howdeterminepwm
Contributor I
Service Request, It's Made, thank yoou!


Message Edited by how determine pwm frequency on 2007-09-20 03:55 PM

Message Edited by how determine pwm frequency on 2007-09-20 03:56 PM
0 件の賞賛
返信