CW7.2 and CW10.1 optimisation performance for Coldfire

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW7.2 and CW10.1 optimisation performance for Coldfire

1,072 次查看
mjbcswitzerland
Specialist V

Hi All

 

Can anyone explain the following?

 

1) I have a reference project that builds with CW7.2, CW10.1 and GCC

2) Each of the compiler targets are set up for maximum optimisation for size (in particular CW7.2 has register passing configured)

3) The code size (that is, the size of the code burned into FLASH) is:

 

CW 7.2 = 82k

GCC = 88k

CW10.1 = 113k

 

I would expect that CW 7.2 be a bit better than GCC but I wonder why CW10.1 is generating 38% more code (28% more that GCC). With decreasing optimisation level the code size goes up, so it is not that it is not trying...

 

Regards

 

Mark

标签 (1)
0 项奖励
回复
1 回复

830 次查看
mjbcswitzerland
Specialist V

Hi All

 

Thanks to Freescale support I compared a few other settings and managed quite an imporvement by setting the following processor options:

 

-          Register coloring

-          Instruction scheduling

-          Peephole

 

The CW10.1 code size is now 84k, which is very close to the CW7.2 code size.

 

Regards

 

Mark

 

0 项奖励
回复