CW10.x and other Eclipse-based IDE's on the same PC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10.x and other Eclipse-based IDE's on the same PC?

Jump to solution
983 Views
FridgeFreezer
Senior Contributor I

I have installed & running CW10.2 on my PC (Windows 7/32) for our main project (Coldfire based).

 

For another project the customer dictates we use Texas MSP430, but when trying to install Code Composer Studio there was a problem / clash (I don't have exact details), and then if I try to uninstall the incomplete thing it says "Uninstalling Eclipse..." which if course I do NOT want to do as that would kill Codewarrior, and lord knows that took long enough to get working...

 

Anyway, getting to the point: Is anyone out there successfully running more than one Eclipse-based IDE on the same PC, and if so can you give any tips on how to install/uninstall without ruining everything? Or if not... er, help!? :smileyindifferent:

Labels (1)
0 Kudos
Reply
1 Solution
755 Views
J2MEJediMaster
Specialist I

That's essentially the same answer for CodeWarrior. You run the installer, and let it put a specific sub-directory in the C:\Program Files\Freescale directory. To uninstall, go to the Start Menu and choose Programs > Freescale CodeWarrior > CW for XXX > Uninstall. Note: This is for a system running Windows XP SP3. Things are going to be different with Windows 7.

 

I've added and removed CodeWarrior with the Eclipse IDE numerous times without problems this way.

 

---Tom

 

 

View solution in original post

0 Kudos
Reply
4 Replies
755 Views
FridgeFreezer
Senior Contributor I

Well I've found an answer to half of my question on Ti's forums - each program installs its own Eclipse folder and should therefore only uninstall its own copy. That certainly seems to have worked for uninstalling Ti's broken software anyway :smileylol:

0 Kudos
Reply
756 Views
J2MEJediMaster
Specialist I

That's essentially the same answer for CodeWarrior. You run the installer, and let it put a specific sub-directory in the C:\Program Files\Freescale directory. To uninstall, go to the Start Menu and choose Programs > Freescale CodeWarrior > CW for XXX > Uninstall. Note: This is for a system running Windows XP SP3. Things are going to be different with Windows 7.

 

I've added and removed CodeWarrior with the Eclipse IDE numerous times without problems this way.

 

---Tom

 

 

0 Kudos
Reply
755 Views
mjbcswitzerland
Specialist V

Hi

 

I have CW10.1, CW10.2, TI CodeComposer 4, Atollic AVR32, Atollic ARM and Atmel AVR32 Studio 2 installed on one Windows 7 PC without any problems. These are all based on Eclipse and haven't disturbed each other during installs/upgrades or when operating.

 

The only possible restriction is when trying to build the same project with two tools - eg. CW10.2 and Atollic ARM. The IDEs litter the project with their own files and .metadata directories. This is less distrubing with newer versions I believe and maybe multiple Eclipse based projects basen on the same project source may collide with some of these - I don't know though because I avoided trying up to now :smileywink:

 

Regards

 

Mark

 

0 Kudos
Reply
755 Views
FridgeFreezer
Senior Contributor I

Thanks guys. Pretty similar feedback from the TI side too - it's just the lack of distinction when an (un)installer says something about changing Eclipse, when you've got more than one thing using Eclipse it can be a bit of a leap of faith that it's not going to change the wrong one!

0 Kudos
Reply