CW10.1 make: *** [Sources/asm_main_asm.obj] Error 1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10.1 make: *** [Sources/asm_main_asm.obj] Error 1

1,611 Views
mylim
Contributor IV

Hi, I have see some others encountering quite a similiar issue as i am facing but I could not find a proper solution for this issue in the forum.

Basically I have tried creating a few new test projects and after messing around the asm_main.asm, MCUinit.asm and main.c in relocatable assembly mode i constantly bump into the similiar problem.

I still couldn't find the root of the issue nor solving it.

Anyone could share please?

Another thing is i do not get the problem in CW6.2 & 6.3 when I copy the code and recreate in the old environment.

Meantime, my CW10.1 and CW6.2 is running on Win7 64-bit which I doubt it's the issue.

Thanks.

 

Regards,

MY

Labels (1)
0 Kudos
Reply
3 Replies

1,417 Views
CrasyCat
Specialist III

Hello

 

Did you try to do a "Clean Project" and then a "Build Project" ?

 

CrasyCat

0 Kudos
Reply

1,417 Views
mylim
Contributor IV

Hi Cat, 

I have tried cleanning it but it doesn't help.

Same error message when I rebuild it. :smileysad:

 

Regards,

MY

0 Kudos
Reply

1,417 Views
stanish
NXP Employee
NXP Employee

hi MY,

 

Could you perhaps click on "Console" Tab to see more information about the error you get?

Could you post  the Console content?

 

Stanish

 

0 Kudos
Reply