CW10.1 - PE does not generate code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW10.1 - PE does not generate code

2,338件の閲覧回数
KevinF
Contributor I

The Processor Expert will not generate code after a new component has been added.  The status area always shows "66%", but afterwards no additional code was added nor any cpu.c modifications made.  It had been working fine for weeks, then mysteriously stopped.

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,892件の閲覧回数
Numerobis
Contributor II

Hi,

I have the same probleme with CW10.1 and device initialization no code is genarate. Also no MCUInit the compilation failed.

0 件の賞賛
返信

1,892件の閲覧回数
Numerobis
Contributor II

Hello,

 

Nobody for answer ? CW10.1 go to the garbage, i work with CW 10.0...

Domi

0 件の賞賛
返信

1,892件の閲覧回数
CrasyCat
Specialist III

Hello

 

I did create a project for HCS08AC8, where I did enable Device Initialization.

I am able to generate code and add devices to configure there.

 

So this seems to be working just fine.

 

I would recommend you to submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.

CrasyCat

0 件の賞賛
返信

1,892件の閲覧回数
Numerobis
Contributor II

Hello,

 

It's ok in win 7 pro64 with "run as administrator":smileyhappy:

 

Domi

0 件の賞賛
返信