CW update

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW update

4,452 Views
bob_s
Contributor III
running CW 8.1.1A

When I checked on updates, I saw an update for 8.2.2.  When I downloaded it, it wouldn't install because it was apparently an upgrade for version 8.2.  Where do I find 8.2?
Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

2,476 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
The last version is DSC 8.2.3.
You can download this version on our web site via the link:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC
For details please have a look in:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC&tab=In-Depth_Tab
In the download tab you can download the Special Edition or the Evaluation.
The Special edition contains the special edition license limited to 32 kb of Code.
We recommend you to download the Evaluation edition.
A Professional Evaluation license is provided for first 30 days.
After 30 days the product will function at the Special Edition level.
If you need another version of the license please contact your local distributor.
You can purchase it directly from the web site too.
We changed the pricing and packaging structure for Codewarrior Tool.
Now there are 4 suites:
 special (free version)
 basic
 standard
 professional
Please refer to the link for details:
http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127262E703BC5
Go to the www.freescale.com and click on My Freescale.
After you were logged, select CodeWarrior Licensing under MY Secure Application.
In the new dialog you can manage your license file.
Keep in mind you can have several versions installed on the same PC.
There is only one restriction: install them on separate folder.
If you're using an old version, please backup your project before to try it with this new version.
If you will meet some compatibility issue you could back to the older version without problem.
Pascal
0 Kudos
Reply

2,476 Views
rbonacina
Contributor I
Hello,
what should I do to upgrade from CW 8.2.2 to CW 8.2.3? I currently have 2 CodeWarrior Standard Suite - Perpetual floating licenses used for CW 8.2.2.

Best Regards,
Roberto

0 Kudos
Reply

2,476 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
Nothing.
Just keep/save your license file.
The license for 8.x is working for 8.0, 8.1, 8.2, .... for 8.x versions.
 
Keep in mind you can have several version installed on the same PC.
In your case you can keep your 8.2.2 and install the 8.2.3 on another folder.
 
Regards
Pascal
0 Kudos
Reply

2,476 Views
rbonacina
Contributor I
OK, but which version should I have to download? The evaluation version or the special edition?

Best Regards,
Roberto
0 Kudos
Reply

2,476 Views
trytohelp
NXP Employee
NXP Employee
As you want.
The tool is the same.
The evaluation contains a 30 day full license.
If you download the evaluation license you will have the full version for 30 days.
After this delay the tool will work in special edition so you will need to put your standard license.
In case of Special edition, you must apply immediatly your standard license.
 
Pascal
0 Kudos
Reply