CW for StarCore crashes during compiling

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW for StarCore crashes during compiling

3,196件の閲覧回数
Quasar
Contributor I

Dears,

My setup is:

CodeWarrior StarCore Compiler (Windows), Engineering Build 22 Service Pack 5

CodeWarrior Development Studio for SC3X00 Architectures, Version 3.1.1, Official Patch, Build 1

IDE Version: 5.7.0 Build 2393

 

I’m facing with a strange issue.

From time to time, the CW for SC3400 crashes during compiling. This is random and hard to reproduce. The project contains about 200 files.

 

I’ve checked for known issues regarding this problem on this forum and I’ve found some clues…

  1. Concurrent compiles should be deactivated. Done
  2. Compiling is done on a dual core processor. It seams that some problems might occur on this PC configuration.
  3. Path length. I made it shorter.
  4. Avoid symbols such as $ in the path. Done
  5. Enough space on local drives. Thanks God … I have plenty …
  6. Office Groove 2007. It was a clean machine… no such software installed.

 

Have you got any kind of problems related with compiler crash in the past?

Do you have any other suggestions?

 

Your help will be appreciated. Thanks.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,593件の閲覧回数
CrasyCat
Specialist III
Hello
 
This needs to be investigated by our support team.
 
I would recommend you to submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.
 
CrasyCat
0 件の賞賛
返信

1,593件の閲覧回数
Quasar
Contributor I
Hi,
 
Thanks a lot.

Unfortunately, I have nothing to report since I do not know the exact cause. Sometimes works sometimes doesn’t.

I’m trying to perform some tests in order to see if it is related with a memory leak issue.

 

Best regards,

0 件の賞賛
返信

1,593件の閲覧回数
Quasar
Contributor I
Hi again,
 
Some updates:
 
I've managed to catch the problem again. Practically, the IDE stops at linking phase.
It shows the message in attachment. I leave it more than 12h and it didn't finished.
 
I've looked in Windows task manager and everything seems to be OK. Plenty of memory available and the processors (I have a dual-core) are not used.
 
Once, I think I've read something on this forum related with a long time linking due to a very big *.xml file. I'm not sure ... i will search.
Any other ideas will be appreciated.
 
Thanks. 
 
 
0 件の賞賛
返信