CW & async baud set

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW & async baud set

2,480件の閲覧回数
bob_s
Contributor III
I've configured an async serial port with a CW bean.  I selected the baud rates I want to be able to select, but the bean does not enable the routine to change the baud rate.  Please see the attachment pics.  Thanks.
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,119件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
To investigate the problem, it will be better to log it directly in the Technical support system.
Please use Freescale on line support web page.
  - Go to following URL: http://www.freescale.com/TechSupport
  - Click on Submit a Service Request. You will come to a login page.
  - You can submit your request through the web from there.
 
Please provide us more details about the Tool version used.
To do that you must:
* CW:
Start the IDE and click on Help | About Metrowerks CodeWarrior.
Click on Installed Products 
Provide us all info displayed.
Or you can save them in a txt file.
 
Can you please provide us your example reproducing the issue ?
 
Pascal
0 件の賞賛
返信

1,119件の閲覧回数
bob_s
Contributor III
Hi Pascal;

Thanks for the response.  What I found was that the routine was enabled, it was just  grayed out because it wasn't a routine that could be optionally excluded.   I thought that because it was grayed out, it couldn't be used.  No problem exists at this point. :smileyhappy:
0 件の賞賛
返信