CW USB TAP: Driver for Windows 10 64-bit System

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW USB TAP: Driver for Windows 10 64-bit System

3,140件の閲覧回数
evanespina
Contributor I

I have installed on my "new" laptop the 56800E Flash Programmer but I get the error "USB open failure" when I try to program the DSP.  The USB TAP device worked the last time I used it, albeit some years ago on an old laptop.  So I'm thinking that the problem now is related to the device driver as the installer I used is also an old one.  Can anyone advise where I can find a link to the latest drivers?  Thanks.

タグ(1)
0 件の賞賛
返信
1 返信

2,359件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Frankly speaking, I use Win7 OS now, I never use Win 10 os, so I can not say the usbtap is okay or not on win 10 os.

Anyway, I copy the usbtap drivers from CodeWarrior for MCU ver 10.7, pls try to install it.

BR

Xiangjun rong

0 件の賞賛
返信