CW 5.9.0 Project file sharing conflict

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW 5.9.0 Project file sharing conflict

1,389 次查看
Mark_A
Contributor I

Hello,

 

I have a project that is shared with 3 developers. 

 

All 3 developers have the identical versions of Codewarrior and service packs installed. 

 

Developer "1" has Windows 7; Developer "2" and "3" have XP. 

 

Developer "1" and "3" open/save the project (project.mcp) in binary format.  Developer "2" can open either format of project file (project.mcp) but only saves the project file (project.mcp) in XML.  Developer "1" and "3" cannot open the XML file (project.mcp) directly, but must rename it and then import it.

 

What must Dev "2" do to save the project file the same format as the others (or vice-versa)?

 

Thanks,

Mark_A

标签 (1)
0 项奖励
回复
2 回复数

1,245 次查看
kef
Specialist I

Are you deleting priject_Data subfolder? I think it must be done when moving project to different machine.

0 项奖励
回复

1,245 次查看
Mark_A
Contributor I

I think I found the problem.  Under IDE Preferences->IDE Extras, Other Settings, "Use text-based projects" was checked.  I didn't see that the first 10 times I looked at it :-\

 

Now it works as expected.

 

Mark_A

0 项奖励
回复