Automation of Boot Sequence for MPC8377WLAN board with code warrior ide 8.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Automation of Boot Sequence for MPC8377WLAN board with code warrior ide 8.0

1,030件の閲覧回数
Sravan_P
Contributor I

Hi,

 

I have a set of binary files to be loaded on to the taget as BOOT sequence. These binary executables (boot) are in development stage and hence a lot of flash erases and re loading are done.

At present,  i am manually erasing and flashing the boot using flash programmer option, i tried searching for command line options like 'erase' or 'program' but could not find any.

It would be helpful if anyone can help how to proceed in automating the boot process (how to load a binary file at a given address) through scripts or anything else .

 

IDE : CodeWarrior 8.0

Target : MPC8377WLAN board

 

Regards

Sravan

ラベル(1)
0 件の賞賛
返信
1 返信

920件の閲覧回数
J2MEJediMaster
Specialist I

Take a look at the information in this https://community.freescale.com/message/53144#53144 on scripting and flash programming.

 

If that information is not suitable, try doing a search on these forums for "Tcl". The command-line debugger present in both the CodeWarrior Classic IDE (some versions) and the CodeWarrior Eclipse IDE supports the execution of Tcl scripts.

 

---Tom

0 件の賞賛
返信