Hi,
I have a set of binary files to be loaded on to the taget as BOOT sequence. These binary executables (boot) are in development stage and hence a lot of flash erases and re loading are done.
At present, i am manually erasing and flashing the boot using flash programmer option, i tried searching for command line options like 'erase' or 'program' but could not find any.
It would be helpful if anyone can help how to proceed in automating the boot process (how to load a binary file at a given address) through scripts or anything else .
IDE : CodeWarrior 8.0
Target : MPC8377WLAN board
Regards
Sravan