Academic Registration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Academic Registration

5,170 Views
Fred37b
Contributor I

Hi,

 

I'm a french student who have to use Codewarrior 8.0 with a DSP56F807. I got an academic licence which i enter on to the freescale internet web site, i put the registration code and i download "CW_DSC56800E_8.3_Evaluation.exe" and the file licence.bat which i put in the codewarrior file, i choose the DISK ID and i put my hard drive referenc.

 

When i start codewarrior IDE il'll go to the menu "Help" in the menu bar and i want to register with the selection "Licence Autorization", i enter the Licence Authorization Codeand i choose the node lock id with disk id but it doesn't work. I can't register my codewarrior.

 

I think i do somthing wrong, but i don't understand what 

Labels (1)
0 Kudos
Reply
8 Replies

3,654 Views
J2MEJediMaster
Specialist I

You no longer use the CodeWarrior menu to perform a registration. You do that on-line at the following web page:

 

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_LICENSE_REGACT&tid=CWH

 

---Tom

0 Kudos
Reply

3,654 Views
Fred37b
Contributor I

Hi thanks for your answer,

When i download the "licence.dat" file and i put it in my codewarrior installation repertory when i try to build a project Codewarrior give me 8 error like that :

Error   : Unable to use the plugin "Metrowerks M56800 C Compiler". It is licensed and a valid license key was not found.
License file does not support this version.
Feature:       Win32_Plugins_DSP56800_Full
Application version > License version: 8.0 > 7.000
License path:  C:\Program Files\Freescale\CodeWarrior for DSC56800E v8.3\license.dat;
FLEXnet Licensing error:-21,126
For further information, refer to the FLEXnet Licensing documentation,
available at "www.macrovision.com".

What i'm supposed to do or install ?

0 Kudos
Reply

3,654 Views
J2MEJediMaster
Specialist I

What version of the operating system are you using, and is it 32- or 64-bit?

 

---Tom

0 Kudos
Reply

3,654 Views
Fred37b
Contributor I

I want to program a DSP 56F807 which is a 16-bit Digital Signal Controllers.

0 Kudos
Reply

3,654 Views
J2MEJediMaster
Specialist I

No, I meant the operating system on the computer hosting the CodeWarrior tools. You might need to file a service request on that. Click here to file a service request. For Category pick Technical Request, and for Topic pick License issues.

 

---Tom

0 Kudos
Reply

3,654 Views
Fred37b
Contributor I
I use Windows XP Professional for 32 bit systems
0 Kudos
Reply

3,654 Views
J2MEJediMaster
Specialist I

Looking at your error message again, its states the version 8 > 7. So, it sounds like you have got the wrong version of the license. That is, you got a version 8 license and are trying to run it with a version 7 copy of CodeWarrior. Or vice-versa. Again, I recommend that you file a service request on this.

 

---Tom

0 Kudos
Reply

3,654 Views
Fred37b
Contributor I
Thank you for your answers i mailed a request and it seems to work now
0 Kudos
Reply