ALIGN directive does not ALIGN code as expected

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ALIGN directive does not ALIGN code as expected

1,739 次查看
admin
Specialist II

I am developing an application using MC68HC908GZ60 and CodeWarrior 6.3.1 in pure relocatable assembly. I have two tables to read. One has 128 of 16-bit entries, the other has 256 of 8-bit entries. I want to locate them on a $00 address boundary (ex: $2100, $2200) and read entries using index register with either

 

mov x+,target_addr

 or

 

ldhx table_addr

 lda <8-bit ADC input>

 tax

 lda ,x

 'ALIGN 256' directive does not align at all and this mistake is clearly seen in

 Project.map as table start addresses are $214C $1E39.

 Why compiler is ignoring my ALIGN directive? What should I do to really ALIGN

 my tables?

 

code snippets:

 

SINETABLE SECTION

  ALIGN $100

 sinetable: dc.w 2146, 2244, 2341, 2438, 2533, 2628, 2721, 2813

  dc.w 2903, 2990, 3076, 3159, 3239, 3316, 3391, 3462

  ...........

 

EXPTABLE SECTION

  ALIGN 256

 exptable: dc.b 0, 0, 0, 0, 0, 0, 0, 1

  dc.b 1, 1, 1, 1, 1, 1, 1, 1

  ............

 

from Project.map :

 - PROCEDURES:

  sinetable 1E39 10 16 2 MOTOR_Code

  VAR00001 1E49 10 16 0 MOTOR_Code

  VAR00002 1E59 10 16 0 MOTOR_Code

 

......

 

exptable 214C 8 8 1 EXPTABLE

  VAR00001 2154 8 8 0 EXPTABLE

标签 (1)
0 项奖励
回复
1 回复

1,167 次查看
CompilerGuru
NXP Employee
NXP Employee

Out of the assembler manual:

*************************************************************************************** ALIGN - Align Location Counter

Syntax

ALIGN <n>

Synonym

None

Description

This directive forces the next instruction to a boundary that is a multiple of <n>, relative to the start of the section. The value of <n> must be a positive number between 1 and 32767. The ALIGN directive can force alignment to any size. The filling bytes inserted for alignment purpose are initialized with `\0'. 

***************************************************************************************

 

I highlighted the part that ALIGN is relative to the start of the section, say it is not aligning relative to the final address.

As the two ALIGN's are both at section offset 0, the alignment is trivially satisfied and nothing gets inserted.

You may want to look into the linker manual, the prm file supports a syntax to align all the section start addresses.

If you just have 2 arrays of known sizes it might also be simpler to allocate them into a specific placement in the prm file instead of allocating them together with the rest of the code.

 

Daniel

0 项奖励
回复