9s08 controller internal EEPROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

9s08 controller internal EEPROM

2,678件の閲覧回数
maddularajesh
Contributor III

Hai , Iam using 9S08DZ60 controller internal EEPROM. while accessing iam getting Access Error.Please kindly suggest the different root causes. I have configured Clock as 200KHZ(PLL Freq is 32MHZ, Selected PRDIV is 1 and DIV factor as 9). Is there any register to be configured for enabling clock. Please kindly share any Software routines available.

Thanks & Regards,

M.N.V.Rajesh

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,418件の閲覧回数
tonyp
Senior Contributor II

In case it helps, I have the following DZ-specific EEPROM library but it's written in macro assembly language:

EEPROM access library in assembly language for 68HCS08 DZ-compatible MCUs

0 件の賞賛
返信

2,418件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

I have a  S08DZ eeprom demo project and doc.

Hope this helps.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信