2 softwares in 1 S19 file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2 softwares in 1 S19 file

2,034件の閲覧回数
gae037
Contributor I
Hello,
 
I have 2 different software and I want to have only 1 file to download. My two software have a data memory area defined for the variable. The first software is located from 0x6C00 to 0x7FFF and the second one is located from 0x4200 to 0x5AFF.
How can I do to have only one file to download?
Thanks in advance for your answers.
 
 
ラベル(1)
0 件の賞賛
返信
1 返信

559件の閲覧回数
CrasyCat
Specialist III
Hello
 
If you want to merge code from two application  (abs file) into one single S19 file, just merge the two .bbl files together.
Can look as follows:
 
Code:
OPENFILE "Appl.s19"format=motorolabusWidth=1origin=0len=0x10000destination=0SRECORD=SxSENDBYTE 1 Appl1.absformat=motorolabusWidth=1origin=0len=0x10000destination=0SRECORD=SxSENDBYTE 1 Appl2.absCLOSE

 
This will merge code from appl1.abs and appl2.abs into a file appl.s19.
 
Use this file as command file in the burner.exe utility.
 
CrasyCat
0 件の賞賛
返信