Hi Team and @john_floros Our team need a UDP transmit/receive example over Ethernet, bare-metal or RTOS, showing how to send an arbitrary byte payload to a specific IP and port. Thanks!
... View more
This keeps track of the issue we found with the current IDE project wizard not generating boot_header.c. This must be resolved for the B0 board.
... View more
Hi team, this is where we can keep track of the information on NPU support. Please let us know if there are working examples/sdk available.
... View more
Hi NXP Team @john_floros , I was trying to perform a loop test with CAN0 and CAN1. In the schematics it shows GPIO81 is the CAN0 RX and GPIO100 is the CAN0 TX. However, in the SDK pin tool this definition is reversed. Do we know if the schematics is wrong? If the schematics is wrong we will just use TX and RX for CAN0 in reverse on the board? Patrick
... View more
The following has evaluated to null or missing:
==> coreNode.discussionStyle [in template "Language_CP_BulkTranslation_Angular" at line 35, column 37]
----
Tip: It's the step after the last dot that caused this error, not those before it.
----
Tip: If the failing expression is known to be legally refer to something that's sometimes null or missing, either specify a default value like myOptionalVar!myDefault, or use <#if myOptionalVar??>when-present<#else>when-missing#if>. (These only cover the last step of the expression; to cover the whole expression, use parenthesis: (myOptionalVar.foo)!myDefault, (myOptionalVar.foo)??
----
----
FTL stack trace ("~" means nesting-related):
- Failed at: #assign interactionStyle = coreNode.d... [in template "Language_CP_BulkTranslation_Angular" at line 35, column 9]
----
Group Hub Information
Amazon - S32K5 Product Support
This community is to provoide technical support to Amazon projects on S32K5