zigbee 13213 sent massege to end device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

zigbee 13213 sent massege to end device

1,946件の閲覧回数
moti
Contributor I
Hi,
Im using 13213 EVK and tring to send data\maseges via uart to the coordinator and to the end device. im reading the 802154MSNAUG file - 2.1.7 Sending Data to the End Devices
but wuthout success
Do somebody know how to do it -please connect and advice.
Thank you,
 
ラベル(1)
0 件の賞賛
返信
1 返信

1,197件の閲覧回数
Mads
Contributor V
Moti,
 
Try programming MyWirelessApp example 5a and b, or 6a and b into 2 boards.
The MyStarNetworkDemo also does the same thing.
Note if you are using low power mode, then try to disconnect the debugger.
Both application set does what you request.
 
BR,
Mads
 
0 件の賞賛
返信