wirelss uart example and chat - ZigBee

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

wirelss uart example and chat - ZigBee

2,397 次查看
fenomeno83
Contributor I
hello...I have 2 12192-evb board...I would use wireless Uart example of beekit to create something like a chat between 2 pc...for do this, it's necessary that 2 board switch from coordinator to end device?because coordinator send message and end device receive...but if device that receive message want send a reply must become coordinator (and the inizial coordinator became the end device?)?
how do this(if is possibile)modifying something in wireless UART example?
thanks

 
 
 
 
 
 
 
 
 
Added ZigBee to the subject.


Message Edited by NLFSJ on 2008-04-18 02:04 PM
标签 (1)
0 项奖励
回复
1 回复

1,199 次查看
addiyi
NXP Employee
NXP Employee
Hello,

I recommend you to try domo application WirelessUART from BeeStack codebase. Using this application, you can send character between two boards, in each sense (from coordinator to end device and from end device to coordinator). Also, for more informations, please read Freescale ZigBee™ Application User’s Guide (ZAUG.pdf), Chapter 5 Creating a Wireless UART application.

Regards,
Adrian

0 项奖励
回复