wirelss uart example and chat - ZigBee

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

wirelss uart example and chat - ZigBee

2,368件の閲覧回数
fenomeno83
Contributor I
hello...I have 2 12192-evb board...I would use wireless Uart example of beekit to create something like a chat between 2 pc...for do this, it's necessary that 2 board switch from coordinator to end device?because coordinator send message and end device receive...but if device that receive message want send a reply must become coordinator (and the inizial coordinator became the end device?)?
how do this(if is possibile)modifying something in wireless UART example?
thanks

 
 
 
 
 
 
 
 
 
Added ZigBee to the subject.


Message Edited by NLFSJ on 2008-04-18 02:04 PM
ラベル(1)
0 件の賞賛
返信
1 返信

1,170件の閲覧回数
addiyi
NXP Employee
NXP Employee
Hello,

I recommend you to try domo application WirelessUART from BeeStack codebase. Using this application, you can send character between two boards, in each sense (from coordinator to end device and from end device to coordinator). Also, for more informations, please read Freescale ZigBee™ Application User’s Guide (ZAUG.pdf), Chapter 5 Creating a Wireless UART application.

Regards,
Adrian

0 件の賞賛
返信