wireless BDM cable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

wireless BDM cable

3,208件の閲覧回数
freegeek
Contributor III
Guys,
 
I have been thinking about developing a wireless bdm tool, it would consist of a USB stick which would communicate to a tiny board which would plug into the target systems BDM 6 pin header.
 
The benefits would be, electrical isolation as well as a tidy workstation.
 
Anyone else think its a good idea?
 
It will only get done if there is a good response.
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,713件の閲覧回数
Nabla69
Contributor V
Hello,
That is good idea.
I wish it to be the same for S08, S12 and CF if possible.
It would be nice to have a universal BDM tool !

Regards,
N.
0 件の賞賛
返信

1,713件の閲覧回数
joerg
Contributor II
I like the idea!
Let me know any details!

Saluti Joerg

PS. since i can now mill my prototypes, it is easier to do any developing!!!

Message Edited by joerg on 2007-01-2402:35 PM

0 件の賞賛
返信

1,713件の閲覧回数
Nouchi
Senior Contributor II
Hi,


It could be a good thing if you choose zigbee transceivers to do that!!
(low cost & low power)
0 件の賞賛
返信