what is the use of filtselect and offset in UINT8 TPMS_READ_ACCELERATION_X(UINT16 *u16UUMA, UINT8 u8Avg, UINT8 u8FiltSelect, UINT8 u8DynamicOffset) ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what is the use of filtselect and offset in UINT8 TPMS_READ_ACCELERATION_X(UINT16 *u16UUMA, UINT8 u8Avg, UINT8 u8FiltSelect, UINT8 u8DynamicOffset) ?

731件の閲覧回数
f20150335
Contributor III

Hi, I am working with the FXTH87xx00 series based on HCS08. In the reference manual the function UINT8 TPMS_READ_ACCELERATION_X(UINT16 *u16UUMA, UINT8 u8Avg,
UINT8 u8FiltSelect, UINT8 u8DynamicOffset) mentions that Filt select selects one of the two filters. What are these filters used for?

In the Offset select table what does this heading "Offset when result of function is 256 counts assuming stand trim.
Span does not change" mean?

Thanks!

タグ(2)
0 件の賞賛
返信
0 返答(返信)