using multiple MC9S08JM60 to program several MC9S08 in parallel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

using multiple MC9S08JM60 to program several MC9S08 in parallel

1,797 次查看
shai_b
Senior Contributor II

Hello team,

My customer plans to build is own programmer JIG for his production line, he plans to flash/program 10 units of MC9S08PA/PL devices in parallel (same firmware). 

Could you please advise what is the best way to build such a JIG, could the customer use multiple #MC9S08JM60 chipsets in order to build such a JIG.

Maybe he can use one MC9S08JM60 device to flash/program several MC9S08x devices in parallel?

waiting for your kind response, thanks in advance.

Regards,

Shai

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,779 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

you can use one JM to program the S08 devices using the OSBDM  and you can download the firmware and the hardware from 

PEmicro | Experts in Embedded tools for Flash Programming and Development 

But I do not know if this can be used in parallel to program several device at the same time

Regards

Vicente Gomez

0 项奖励
回复