using multiple MC9S08JM60 to program several MC9S08 in parallel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

using multiple MC9S08JM60 to program several MC9S08 in parallel

2,357件の閲覧回数
shai_b
Senior Contributor II

Hello team,

My customer plans to build is own programmer JIG for his production line, he plans to flash/program 10 units of MC9S08PA/PL devices in parallel (same firmware). 

Could you please advise what is the best way to build such a JIG, could the customer use multiple #MC9S08JM60 chipsets in order to build such a JIG.

Maybe he can use one MC9S08JM60 device to flash/program several MC9S08x devices in parallel?

waiting for your kind response, thanks in advance.

Regards,

Shai

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

2,339件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

you can use one JM to program the S08 devices using the OSBDM  and you can download the firmware and the hardware from 

PEmicro | Experts in Embedded tools for Flash Programming and Development 

But I do not know if this can be used in parallel to program several device at the same time

Regards

Vicente Gomez

0 件の賞賛
返信