unknown processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

unknown processor

2,435 Views
Tony19
Contributor I

Hi Guys, trying to re-write eeprom on this chip, but cant find the type?.

Its:- KQQMC9543D

I've got most interfaces etc to get into most chips in this era, but bogged down a bit here.

Thanks in anticipation.

T.

Labels (1)
0 Kudos
Reply
3 Replies

1,847 Views
Tony19
Contributor I

Oh dear no response. I've had another look, its 68 pin type looks to be running at 12 mhz. Pins seem to be same as 68HC11 txd, rxd, xtal pins are the same. no-one?

I'll have to put a 4mhz xtal in there and try something.

T.

0 Kudos
Reply

1,847 Views
bigmac
Specialist III

Hello, and welcome to the forum.

 

This component does not follow the normal nomenclature for 8-bit MCUs.  It is possible that it may be a proprietry device manufactured for a specific customer.  It is also quite possible that the device may not be re-programmable.

 

Regards,

Mac

 

0 Kudos
Reply

1,847 Views
Tony19
Contributor I

Thanks for then input Mac, its in a cars ecu, so the eeprom should be programmable/erasable. my software works mainly on 4 & 8 mhz clocks, so I'll try a crystal change.

Tony

0 Kudos
Reply