unknown processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

unknown processor

2,366件の閲覧回数
Tony19
Contributor I

Hi Guys, trying to re-write eeprom on this chip, but cant find the type?.

Its:- KQQMC9543D

I've got most interfaces etc to get into most chips in this era, but bogged down a bit here.

Thanks in anticipation.

T.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,778件の閲覧回数
Tony19
Contributor I

Oh dear no response. I've had another look, its 68 pin type looks to be running at 12 mhz. Pins seem to be same as 68HC11 txd, rxd, xtal pins are the same. no-one?

I'll have to put a 4mhz xtal in there and try something.

T.

0 件の賞賛
返信

1,778件の閲覧回数
bigmac
Specialist III

Hello, and welcome to the forum.

 

This component does not follow the normal nomenclature for 8-bit MCUs.  It is possible that it may be a proprietry device manufactured for a specific customer.  It is also quite possible that the device may not be re-programmable.

 

Regards,

Mac

 

0 件の賞賛
返信

1,778件の閲覧回数
Tony19
Contributor I

Thanks for then input Mac, its in a cars ecu, so the eeprom should be programmable/erasable. my software works mainly on 4 & 8 mhz clocks, so I'll try a crystal change.

Tony

0 件の賞賛
返信