unknown processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

unknown processor

2,340 次查看
Tony19
Contributor I

Hi Guys, trying to re-write eeprom on this chip, but cant find the type?.

Its:- KQQMC9543D

I've got most interfaces etc to get into most chips in this era, but bogged down a bit here.

Thanks in anticipation.

T.

标签 (1)
0 项奖励
回复
3 回复数

1,752 次查看
Tony19
Contributor I

Oh dear no response. I've had another look, its 68 pin type looks to be running at 12 mhz. Pins seem to be same as 68HC11 txd, rxd, xtal pins are the same. no-one?

I'll have to put a 4mhz xtal in there and try something.

T.

0 项奖励
回复

1,752 次查看
bigmac
Specialist III

Hello, and welcome to the forum.

 

This component does not follow the normal nomenclature for 8-bit MCUs.  It is possible that it may be a proprietry device manufactured for a specific customer.  It is also quite possible that the device may not be re-programmable.

 

Regards,

Mac

 

0 项奖励
回复

1,752 次查看
Tony19
Contributor I

Thanks for then input Mac, its in a cars ecu, so the eeprom should be programmable/erasable. my software works mainly on 4 & 8 mhz clocks, so I'll try a crystal change.

Tony

0 项奖励
回复