transfer data via usb interface with jb16

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

transfer data via usb interface with jb16

4,799 Views
fredycolombia
Contributor I

Hi all
I was working  with jb16 to get data and transfer data, I was searching in tbdml and osbdm, but I can't find one code that can compile, also  I only need to transfer data, no need programing the flash or anything else.
I'm going to attach the firmware that I used and prints about the advertisment in windows when I connect the usb to the pc.
I used the driver provided by theyscon, but  it no works.
thanks for your help

regards
fredy

 

instalacion_driver_usb.zip

tbdml_with_jb16.zip

Message Edited by t.dowe on 2009-09-22 11:42 AM
Labels (1)
0 Kudos
Reply
5 Replies

2,802 Views
Luc_sur
Contributor I

This book is great: USB Complete Everything You Need to Develop Custom USB Peripherals. I'm study USB with this book.

 

regards.

0 Kudos
Reply

2,802 Views
joerg
Contributor II
Hi fredy
if it helps i can send you the osbdm source that compiles (with only few warnings!)

Saluti Joerg
0 Kudos
Reply

2,802 Views
fredycolombia
Contributor I
hi
ok there is no problem, please send me the file. Is for jb16?  maybe you know how I can use this firmware to transfer data via usb? can you help me with the driver for windows?  Can I use this firmware only with the mcu jb16 and usb conected to the pc?
I really  appreciate your help.


regars
fredy
0 Kudos
Reply

2,802 Views
joerg
Contributor II
Dear fredy
The software of the osbdm is written for the JB16. It could serve to show you how it works, but the windows driver is for the CW and not open source.

I am not the specialist for writing USB stuff, but if you think the source could be helpful, then please send me a private message with your email address.

Saluti Joerg
0 Kudos
Reply

2,802 Views
fredycolombia
Contributor I
hi
Thanks for  your help joerg, I already send my adress mail.
If someone knows how I can  solve my problem I really be helpful.
 
 
regards
fredy
0 Kudos
Reply