Hello Steve,
The current draw will increase by the following nominal amounts should the particular peripherals remain active during stop mode:
Internal frequency reference 70 uA
LVD module 100 uA
Voltage comparator 20 uA
ADC module 106 uA
Additionally, if the latter modules make use of the internal bandgap reference, there will be a further unspecified current adder. You will need to check which peripherals remain enabled during stop mode.
There should not be a significant difference whether negative edge with pull-up enabled is used, or there is a positive edge with pull-down used for the keyboard input.
For the unused pins, a further alternative is to set the pins to output, and set the output levels low, although there should be little difference in current draw between the methods.
Regards,
Mac