stack ram in 9s08JM60, JM32

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

stack ram in 9s08JM60, JM32

跳至解决方案
1,973 次查看
donw
Contributor IV

Hi all

A strange thing!

I have the stack pointer set to $1000, to use the top end of the 4K ram in the 9S08JM60.

The same code runs in the JM32 part, even though it is supposed to have only 2K ram (ending  at $0800) !

Maybe this part has the ram but is not production verified?

Any one know?

标签 (1)
0 项奖励
回复
1 解答
1,560 次查看
peg
Senior Contributor IV

Hello,

 

It is very common in the early months of production for smaller devices to actually have the die from a larger device.

This has been verified as being so on many different models.

Supposedly Freescale only test the quoted amount of memory.

Generally it stops being like this at some indeterminate point.

So enjoy it while you can!

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,561 次查看
peg
Senior Contributor IV

Hello,

 

It is very common in the early months of production for smaller devices to actually have the die from a larger device.

This has been verified as being so on many different models.

Supposedly Freescale only test the quoted amount of memory.

Generally it stops being like this at some indeterminate point.

So enjoy it while you can!

 

0 项奖励
回复