stack ram in 9s08JM60, JM32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

stack ram in 9s08JM60, JM32

ソリューションへジャンプ
1,996件の閲覧回数
donw
Contributor IV

Hi all

A strange thing!

I have the stack pointer set to $1000, to use the top end of the 4K ram in the 9S08JM60.

The same code runs in the JM32 part, even though it is supposed to have only 2K ram (ending  at $0800) !

Maybe this part has the ram but is not production verified?

Any one know?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,583件の閲覧回数
peg
Senior Contributor IV

Hello,

 

It is very common in the early months of production for smaller devices to actually have the die from a larger device.

This has been verified as being so on many different models.

Supposedly Freescale only test the quoted amount of memory.

Generally it stops being like this at some indeterminate point.

So enjoy it while you can!

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,584件の閲覧回数
peg
Senior Contributor IV

Hello,

 

It is very common in the early months of production for smaller devices to actually have the die from a larger device.

This has been verified as being so on many different models.

Supposedly Freescale only test the quoted amount of memory.

Generally it stops being like this at some indeterminate point.

So enjoy it while you can!

 

0 件の賞賛
返信