s19 File Layout

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s19 File Layout

11,896 Views
bfac
NXP Employee
NXP Employee
Hi!

Anybody has the s19 file layout?

For example, what means the first byte on the first line, and so on...

Thanks a lot!

Bfac
Labels (1)
0 Kudos
Reply
4 Replies

9,423 Views
bigmac
Specialist III
0 Kudos
Reply

9,423 Views
bfac
NXP Employee
NXP Employee
Thanks bigmac!!
0 Kudos
Reply

9,423 Views
JaimeR
Contributor III
I was looking for information about this and since the links above are broken, this is an explanation to s19 file I found:
Motorola S19 file records are a text representation of Hexadecimal coded binary data.
 All data uses only ASCII characters, so the format is portable across virtually all computer
 platforms. The S19 format, described here, is for eight bit data. (The '$' will be used
 throughout to indicate a hexadecimal value.)
Each line in a Motorola S19 file is called a 'record'. Records always begin with a the letter 'S',
 followed by a '1' if the record contains data, or a '9' if this is the last record in the file.
The next byte represents the number of bytes in this record, including the starting address,
 data bytes, and the checksum.
The next pair of numbers represent the 16-bit starting address of the data in the record.
 This is the absolute location in the EPROM.
 Following the address are the hex representations of the data to be stored. The last byte is
 an eight-bit one's-complement checksum of all of the bytes in the record (not including the S1).
 Note that this value is derived from the binary values of the bytes, not the ASCII representation.
A standard CR/LF pair (carriage return/linefeed, $0D $0A) terminates each line.
This a sample Motorola S19 record.
S1130170707172737475767778797A7B7C7D7E7F03
Broken down, it looks as follows:
S               - Indicates that this is Motorola
1               - 1 means this is a data record
13              - Number of bytes to follow = $13, or 19 decimal. This number
                 can be thought of as the number of data bytes plus three.
                Therefore there will be 16 data bytes in the record.
0170            - Starting address in the EPROM for this record.
70              - These are the data bytes (in hex) - 16 of them as noted above
71                The first byte ($70) will be stored at $0170, with the
72                remaining bytes following in sequence.
73
74
75
76
77
78
79
7A
7B
7C
7D
7E
7F
03              - This is the checksum. If you add all of the successive bytes
                 (note that the address is treated as two individual bytes) the
                 result is $7FC. Truncating this to eight bits yields $FC. The
                 one's complement of $FC is $06. (This may be derived by
                subtracting $FC from $FF, or by inverting the bits.)

(CR/LF)         - End of this record -- I think the linefeed may be optional.

The use of the starting address in each record makes it possible to store data in
 non-contiguous areas of the EPROM. Each line of data is therefore entirely self-contained.
This is useful when areas of the EPROM are unused, as no space in the Motorola S19
 file need be wasted by representation of blank data. It is perfectly possible, albeit
 not recommended, to scramble all of the record lines in a Motorola S19 file and still
 end up with a correct EPROM image.

The end record (end of file) is almost the same:
S9030000FC
S               - Indicates that this is Motorola
9               - 9 means this is the end record
03              - Number of bytes - should be three, as no data bytes will be in
                this record.
0000            - Address, usually zero.
              - Zero data bytes here (obviously)
FC              - The checksum, calculated as above.
You may also see records starting with S0 - I believe these are called comment records.
 They do not contain any data that will be stored in the EPROM.

http://www.softhelp.ru/fileformat/s19/s19.htm


9,423 Views
peg
Senior Contributor IV
Hi,

A still current net reference for this.
Looks like this may soon go away so here it is again


Message Edited by peg on 2009-01-14 02:45 PM
0 Kudos
Reply