s08sh bus clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

s08sh bus clock

跳至解决方案
3,783 次查看
PW_CTL
Contributor III

Hi, 

 

I am running an small applicattion with massive SPI data transfers, and I need to improve the speed of this application. There are only a few lines of code, so I am trying to set the s08Sh at its maximum speed.

 

I am using the internal clock, and I followed next steps:

- Internal bus clock is set at 16MHz.

- Trim frequency at   39062,50.

 

Is there something more to do in order to improve the speed of the code?

 

Thanks.

标签 (1)
0 项奖励
回复
1 解答
3,590 次查看
rocco
Senior Contributor II

Hi PW_CTL,

 

You do not need to re-write your code in assembly language. Instead you can look at the assembly language that was generated by your C code (But I don't know the CodeWorrier option to do that). That way, you should be able to optimize your C code to produce the results you need.

 

What bit-rate do you have the SPI programmed for? What's at the other end?

 

I have not used the SH family, but the clock module looks similar to the others that I have used. So it looks like you can run the clock in FEI mode (FLL Engaged Internal), program the FLL to get a 40 MHz DCOOUT clock, which would give you a 20 MHz bus clock.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,591 次查看
rocco
Senior Contributor II

Hi PW_CTL,

 

There may be a number of things you can do.

 

First, is there any reason you are not running at 20 MHz instead if 16 MHz? That would be a 25% improvement.

 

Is your code written in C or assembly language?

Are you running polled or with interrupts?

 

I'm running older HC08GP32 MCUs at 8 MHz, and I am able to sustain the SPI's maximum transfer rate of 4 MHz (a byte every two microseconds) between MCUs. So I see no reason why you shouldn't be able to do that with an S08 at 16 MHZ.

0 项奖励
回复
3,591 次查看
PW_CTL
Contributor III

Hi rocco, thanks for your reply.

 

I am using processor expert to set up the microcontroller and C code with codewarrior.

 

As I told you, my application is very small, running in a small loop of only 4-5 lines of c code. I am not using interrupts.

 

Now, I am reading about 70kbytes/s which is not enough for my purposes. For your comments, there is a problem on my code. I will try to write the main loop in assembly code and check if there is any improvement, but I am not used to write assembly.

 

About the 20-16MHz, the low-power oscillator can bet set between 2 and 16MHz (my mcu is powered at 3.3V). How to reach the 20MHz? Do I need an external oscillator? 

0 项奖励
回复
3,590 次查看
rocco
Senior Contributor II

Hi PW_CTL,

 

You do not need to re-write your code in assembly language. Instead you can look at the assembly language that was generated by your C code (But I don't know the CodeWorrier option to do that). That way, you should be able to optimize your C code to produce the results you need.

 

What bit-rate do you have the SPI programmed for? What's at the other end?

 

I have not used the SH family, but the clock module looks similar to the others that I have used. So it looks like you can run the clock in FEI mode (FLL Engaged Internal), program the FLL to get a 40 MHz DCOOUT clock, which would give you a 20 MHz bus clock.

0 项奖励
回复
3,591 次查看
PW_CTL
Contributor III

Thanks rocco.

 

when I was reviewing the code in assembly, I found something wrong on my own code in C. Well, not really wrong but very inefficient, in the way it is translated to assembly. I fixed that and the speed of my applicattion is now about twice than I need!

 

Thank you very much for your help and advices.

0 项奖励
回复