qg8 stand alone

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

qg8 stand alone

2,742 Views
bradstew
Contributor I
hi,
Have QG8 dev board.
Sometimes I cannot run the board stand alone.  I have to start the program with the debugger attached.  I've tried using an external power supply with no effect.
 
Is there something I need to do to get the part to run in stand-alone mode?  My latest application uses RTI.
 
Thanks
Labels (1)
0 Kudos
Reply
2 Replies

1,450 Views
peg
Senior Contributor IV

Hi bradstew,

The short answer is: No.

Has the problem only occurred on your "latest application"?

Regards David

 

0 Kudos
Reply

1,450 Views
UK_CF_FAE
NXP Employee
NXP Employee
Hi BradStew,
 
Sorry to state something obvious, but did you move jumper PWR_SEL to provide power from the power input jack, rather than from the USB port?
 
Mark
0 Kudos
Reply