programming adapter (PAS08W1628T28E) setup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

programming adapter (PAS08W1628T28E) setup

1,688件の閲覧回数
aurora
Contributor I

I am using a PAS08W1628T28E programming adapter, this adapter is connected to a
P&E cyclone pro through MON08 interface. Also, the P&E cyclone pro is connected
to a PC USB port. The MCU is MC908QC8 (28 pin TSSOP). I have connected jumpers
from J3 to J6 on the programming adapter board (PAS08W1628T28) by one to one
connection (J3-1 to J6-1, J3-2 to J6-2,…….. J3-16 to J6-16). When I run
Codewarrior 6.2, it shows a message “Could not measure target baudrate”. P&E
Connection Manager window shows “Connection Status Summary YNNNN”. Have I
missed other jumper connections? what I have done wrong? P&E cyclone pro is
working correctly when it connects to a 908Q programming adapter (Slicon
Engines).

Thanks,

aurora

ラベル(1)
0 件の賞賛
返信
1 返信

1,417件の閲覧回数
aurora
Contributor I

The problem has resolved.

 

Thanks all.

 

Aurora

0 件の賞賛
返信