programming HCS08s with CW 5.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

programming HCS08s with CW 5.1

5,721 Views
baddad
Contributor I
Is there a way to launch the programmer in CW 5.1 without using the debugger?
 
Thanks,
BadDad
Labels (1)
0 Kudos
Reply
7 Replies

3,203 Views
peg
Senior Contributor IV
Hi BadDad,
 
Other modules can be run independantly, but as the programmer is sold as a standalone product by P&E I believe they have deliberately prevented you from doing this.
 
Regards
David
 
0 Kudos
Reply

3,203 Views
bigmac
Specialist III
Hello Peg,
 
I thought it was possible to run burner.exe as a stand-alone utility - and seem to be able to do so.  Are there other problems that occur once the program is running?
 
Regards,
Mac
 
0 Kudos
Reply

3,203 Views
peg
Senior Contributor IV
Hi Mac,
 
Yes you can run burner.
But what exactly can it burn and through what interface?
This question is about S08!
I have never really looked into this thing properly.
 
Regards
David
 
0 Kudos
Reply

3,203 Views
CrasyCat
Specialist III
Hello
 
burner.exe cannot be used to program flash.
This utility has been designed to convert an ELF DWARF executable file to a S record or Intel Hex file.
 
The burmer does not include any flash programming algorithm.
If you are looking for a production flash programming tool, I would also recommend using P&E or Softec production flash programming tools.
This mainly depends on the connection cable you are using for debugging.
 
CrasyCat
0 Kudos
Reply

3,203 Views
peg
Senior Contributor IV

Hi CrasyCat

From the Burner Help:

The burner utility has:

  • Powerful User Interface
    • On-line Help
      • Flexible Message Management
        • 32bit Application
          • Generation of S-Record files, Binary or Intel Hex files
            • Splitting up application into different EEPROMS (1, 2 or 4 bytes bus width)
              • Both interactive (GUI) and batch language interface (Batch Burner)
                • Batch Burner Language with:baudRate, busWidth, CLOSE, dataBit, destination, DO, ECHO, ELSE, END, FOR, format, header, IF ,len, OPENCOM, OPENFILE, origin, parity, PAUSE, SENDBYTE, SENDWORD, SLINELEN, SRECORD, swapByte, THEN, TO , undefByte.
                  • Supports Freescale (former Hiware) and ELF/DWARF Object File Format, S-Records and Intel Hex Files as input
                    • Supports a serial programmer attached to serial port with various configuration settings
                      • Powerful batch burner language with various commands (fillByte, origin, destination, range, baudRate, header, ...)

                        What is the "serial programmer" that it supports then?

                        Regards
                        David

                         

                        0 Kudos
                        Reply

                        3,203 Views
                        CrasyCat
                        Specialist III
                        Hello
                           This is a legacy feature.
                           The serial programmer referenced there was for programming through an EPROM programmer.
                          
                          As far as I know burner is not used that way any more since a long time.
                          The burner does not include any flash programmer algorithm.
                         
                        CrasyCat
                        0 Kudos
                        Reply

                        3,203 Views
                        ok2ucx
                        Contributor IV

                        Dears,

                        maybe this thread may be of your interest - it's about using HIWAVE (and P&E DLLs) in command line for burning:

                        http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&message.id=75

                        I actually have never tried it...
                         
                        Regards, Pavel (ok2ucx)
                        0 Kudos
                        Reply