program flash in debug mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

program flash in debug mode

3,393件の閲覧回数
IlConte
Contributor IV

I use MC9S08PT60 and CW 10.3.

During debug mode with USM multilink, I need to program a flash sector with data value in a S19 file.

My application is at address 0x1040 and i want program the flash from 0x3200 to 0x4000 with Debug active

Using "Flash file to target" is also erased the flash, but i want to wrtite only a flash sector fron 0x3200 to 0x4000 withot delete the other sector in debug mode.

How can i do this ?

 

Thanks

 

Stefano

15021_15021.pngpastedImage_2.png

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,201件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Stefano,

i ever use CW program some sectors for K40. i think the method is also work for s08.

see attached.

==================================

this answer is for you, if it helps, please click on "Correct Answer" button. thanks!

Best Regards.

Zhang Jun

0 件の賞賛
返信

3,201件の閲覧回数
IlConte
Contributor IV

Thanks, when i select the "Import Task" menu i insert the PT60 xml file but afer nothing happens !!

Probably something wrong

Thanks

0 件の賞賛
返信