pls. advice on the programmer kit for MC9S08QE128 .  we are developing BPM, using freescale design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pls. advice on the programmer kit for MC9S08QE128 .  we are developing BPM, using freescale design

1,049 Views
jagannathang
Contributor II

can anybody advice us the program tools, and setup kits for programming and copying programs to MCU.  PLS. ADVICE PART NO and also the availability

Labels (1)
0 Kudos
Reply
2 Replies

921 Views
tonyp
Senior Contributor II

P&E Micro's Cyclone PRO​  is a great solution for quick programming (if you plan to do a lot of units fast).  Stand-alone programming, i.e., no PC connection required!

A much cheaper (but also slower for larger volume production) solution is the various USBDM

0 Kudos
Reply

921 Views
jagannathang
Contributor II

Dear Mr. Tony,

thanks. can u pls. help me with the specs of the VAlve, and the Motor , specified in the block diagram of BPM machine.

regads

jagan

9845497950

G.Jagannathan

MANAGING DIRECTOR

AARMS Value Chain Pvt. Ltd.,

#211 D, I Floor, Temple Street,

9th Main Road, BEML III Stage,

Rajarajeshwari Nagar,

Bangalore- 560098

mob : 9845497950

www.aarmsvaluechain.com

0 Kudos
Reply